:REPository:SERVer:VERSion?
Meas. mode:
Scope
Eye
Jitter
TDR
Publish mode:
Selected
Custom
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:REPository:SERVer:VERSion?
Query Response
For example, "2.0.0-123
".
Description
Returns the current version of the N8844A data repository server. Before sending this command, a connection must be established to the server using the :REPository:CONNect
command.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.