:REPository:CONNect:STATe?
Meas. mode:
Scope
Eye
Jitter
TDR
Publish mode:
Selected
Custom
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:REPository:CONNect:STATe?
Query Response
{CONN | NCON}
Description
Queries the current state of the connection of FlexDCA to an N8844A data repository server. Use the :REPository:CONNect
command to make the connection. The following responses can be returned:
- CONN
- Server is connected.
- NCON
- Server is not connected.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.