:REPository:DISConnect
Meas. mode:
Scope
Eye
Jitter
TDR
Publish mode:
Selected
Custom
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:REPository:DISConnect
Description
Disconnects FlexDCA from an N8844A data repository server. Measurement data can not be uploaded to the server until the connection is re-established using the :REPository:CONNect
command. You can check the status of the connection using the :REPository:CONNect:STATe?
query.
Use of an *OPC?
query to pause program execution while waiting for this command to execute.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.
Example Command Sequence
:REPository:DISConnect *OPC?