:REPository:PUBLish
Meas. mode:
Scope
Eye
Jitter
TDR
Publish mode:
Selected
Custom
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:REPository:PUBLish
Description
Publishes the currently selected measurement data to the specified data set on an N8844A data repository server. Use the :REPository:DSET
command to specify the data set, which is a folder of the N8844A. Use the :REPository:CANCel
command to cancel the data transfer.
If the measurement fails to publish, check that:
- The server is still connected, and
- A data acquisition has occurred since the last publish.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.
Example Command Sequence
:REPository:CONNect // Connect to server :REPository:DSET "FlexDCA" // Upload to this folder :REPository:DUT:MODel "DUT_53" :REPository:DUT:SERial "US0012345" :REPository:MEASure:SELection:CLEar // Define data to upload :REPository:MEASure:PAM:LEVel:SELection:ALL :REPository:MEASure:PAM:EYE:SELection:ALL :REPository:MEASure:PMODe SELected :REPository:PUBLish // Upload data :REPository:DISConnect