:TDR:DUT:STATus:REASon

Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter

Query Syntax

:TDR:DUT{1:16}:STATus:REASon?

Where {1:16} indicates one of 16 possible DUT setups.

Description

Returns a string that explains the reason for a failed TDR DUT setup. An example return string would be "You must connect at least one TDR channel to this DUT to make measurements.". If the setup is correct, a null string is returned. Use the STATus? query to determine the state of the setup.

Requires FlexDCA revision A.04.00 and above.