:TIMebase:RTSCope:INTerpolate:AUTO

Instrument
UXR Scope
Flex Apps:
N1010A
FlexRT
License:
L-RND
Meas. mode:
Scope
Eye

Command Syntax

:TIMebase:RTSCope:INTerpolate:AUTO {ON | OFF}

Query Syntax

:TIMebase:RTSCope:INTerpolate:AUTO?

Description

Selects automatic Interpolation used in FlexRT's waveform acquisition on or off. The equivalent GUI setting is located the the Infiniium Scope Setup dialog's Acquisition tab. By default, automatic is selected.

When automatic Interpolation is turned off, you can select either Sin(x)/x interpolation or no interpolation with the :TIMebase:RTSCope:INTerpolate:METHod command. When Sin(x)/x is used, use the following commands to configure the interpolation. These settings are linked, so changing either setting changes the other setting:

(acquired samples-per-UI) (factor) = samples-per-UI

This acquisition setting is automatically shared with all UXR oscilloscope input channel waveforms.

Requires FlexDCA revision A.06.70 and above.