:TIMebase:RTSCope:UI:Range
Instrument
UXR Scope
Flex Apps:
N1010A
FlexRT
License:
L-RND
Meas. mode:
Scope
Eye
Command Syntax
:TIMebase:RTSCope:UIRange <unit intervals>
<unit intervals> is a double.
Query Syntax
:TIMebase:RTSCope:UIRange?
Description
Sets the number of Unit Intervals (UIs) displayed across the graticule's horizontal axis, when the timebase units are set to UIs (:TIMebase:UNITs). Use :TIMebase:UIPosition to set the UI delay.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.
Requires FlexDCA revision A.06.70 and above.