:TIMebase:RTSCope:INTerpolate:METHod
Instrument
UXR Scope
Flex Apps:
N1010A
FlexRT
License:
L-RND
Meas. mode:
Scope
Eye
Command Syntax
:TIMebase:RTSCope:INTerpolate:METHod {NONE| SINC}
Query Syntax
:TIMebase:RTSCope:INTerpolate:METHod?
Description
Selects sin(x)/x interpolation or selects no interpolation.
- SINC
- Selects the sin(x)/x method, which is the default and is preferred when reconstructing a signal (having evenly spaced samples) that has been band limited. The number of points in the output waveform are evenly spaced and are set by either the interpolation factor (
:TIMebase:RTSCope:INTerpolate:FACTor) command or the samples-per-UI (:TIMebase:RTSCope:INTerpolate:SPUI) command. - NONE
- Turns interpolation off.
This acquisition setting is automatically shared with all UXR oscilloscope input channel waveforms. To independently configure for specific channels, use the :CHANnel:RTSCope:TRACk command.
Requires FlexDCA revision A.06.70 and above.