:TIMebase:RTSCope:SPUI?
Instrument
UXR Scope
Flex Apps:
N1010A
FlexRT
License:
L-RND
Meas. mode:
Scope
Eye
Query Syntax
:TIMebase:RTSCope:SPUI?
Description
Returns the number of Acquired Samples / UI in the UXR oscilloscope's input waveform. The equivalent value is displayed in the FlexRT Infiniium Scope Setup dialog's Acquisition tab for waveform interpolation. Use the following commands to configure the interpolation:
:TIMebase:RTSCope:INTerpolate:AUTO. Turns on or off automatic configuration of waveform interpolation.:TIMebase:RTSCope:INTerpolate:FACTor. Specifies a factor (integer value) that determines the number of points FlexRT uses to interpolate between points on the real-time oscilloscope's waveform.:TIMebase:RTSCope:INTerpolate:METHod. Selects either sin(x)/x interpolation or selects no interpolation.:TIMebase:RTSCope:INTerpolate:SPUI. Specifies a samples-per-UI that FlexRT uses to determine the number of points on the real-time oscilloscope's interpolated waveform.
Requires FlexDCA revision A.06.70 and above.