:TIMebase:RTSCope:UIRange:AUTO
Instrument
UXR Scope
Flex Apps:
N1010A
FlexRT
License:
L-RND
Meas. mode:
Scope
Eye
Command Syntax
:TIMebase:RTSCope:UIRange:AUTO {ON | OFF}
Query Syntax
:TIMebase:RTSCope:UIRange:AUTO?
Description
Turns on or off the automatic setting of the Acquisition Range for UXR oscilloscope input waveforms. This command is linked to the :TIMebase:RTSCope:XRANge:AUTO command and either command can be used.
To return the current acquisition range use the :TIMebase:RTSCope:UIRange? (for Unit Interval) and :TIMebase:RTSCope:XRANge? (for seconds) queries. When the automatic setting is off, set the range using the :TIMebase:RTSCope:UIRange(for Unit Interval) and :TIMebase:RTSCope:XRANge(for seconds) commands.
To select which acquisition range units are displayed in the FlexRT Infiniium Scope Setup dialog, use the :TIMebase:UNITs command.
Requires FlexDCA revision A.06.70 and above.