:TIMebase:RTSCope:INTerpolate:FACTor

Instrument
UXR Scope
Flex Apps:
N1010A
FlexRT
License:
L-RND
Meas. mode:
Scope
Eye

Command Syntax

:TIMebase:RTScope:INTerpolate:FACTor <factor>

<factor> is an integer.

Query Syntax

:TIMebase:RTScope:INTerpolate:FACTor?

Description

Specifies a factor (integer value) that determines the number of points FlexRT uses to interpolate between points on the real-time oscilloscope's waveform. To select the interpolation method, use the :TIMebase:RTScope:INTerpolate:METHod command. The number of sample-per-UI in the interpolated waveform is:

(acquired samples-per-UI) (factor) = samples-per-UI

You can also directly set the sample-per-UI using the :TIMebase:RTScope:INTerpolate:SPUI command.

This acquisition setting is automatically shared with all UXR oscilloscope input channel waveforms. To independently configure for specific channels, use the :CHANnel:RTSCope:TRACk command.

Requires FlexDCA revision A.06.70 and above.