:CHANnel Interpolation & Range Commands (FlexRT)
Instrument
UXR Scope
Flex Apps:
N1010A
FlexRT
License:
L-RND
Meas. mode:
Scope
Eye
Use these :TIMebase:RTSCope subsystem commands to configure how FlexRT interpolates and samples all Infiniium channel waveforms. In the GUI, these universal settings are made in the Infiniium Scope Setup dialog.
For any selected channel, you can disable or enable these universal (shared) settings so that the channel can have its own unique setting. To do this, use the :CHANnel:RTSCope:TRACk command.