Infiniium Connection Setup Dialog
When N1010A FlexDCA is installed on a PC, the Infiniium Connection Setup dialog allows you to connect FlexDCA to a Keysight UXR-series oscilloscope, which also enables N1010A FlexDCA's FlexRT capability. In the dialog's Hostname field, enter the computer name for the Infiniium UXR-series oscilloscope on the LAN.
This menu command is only available when FlexDCA is installed on a PC. This menu command is not available from FlexDCA running on a DCA-X. When FlexDCA is installed on the Infiniium UXR-series oscilloscope, the connection is established by clicking Analyze > Launch FlexRT on the UXR oscilloscope's menu.
While FlexDCA running on a PC is connected to a UXR-series oscilloscope, FlexDCA cannot acquire data from any other source. For example, a simulated module, a module installed in a DCA-X, or a DCA-M module.