Extended Module Configuration Dialog
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Use the Extended Module Configuration dialog to connect FlexDCA to following hardware:
- DCA-X from FlexDCA N1010A on PC (Flex-on-Flex connection) Setup dialog.
- Keysight UXR Oscilloscope Setup dialog.
- Keysight DCA-M module Setup dialog.
- Keysight Arbitrary Waveform Generator Setup dialog.
- Optical switches Setup dialog.
- Simulated optical and electrical receiver modules Setup dialog.
Click Setup > Configure Extended Modules to open this dialog. Or, click the
icon that is displayed to the right of the channel buttons along the bottom of the display.
- Click the Hardware or Simulation tab, find the picture of the item that you want to connect, and drag the picture to a FlexDCA "slot" location as shown in the following picture.
- Click on the picture in the slot location to open a Connection Setup dialog from which you can make the connection. The following picture shows the dialog that is used to setup a Flex-on-Flex connection to a DCA-X.