Minimum

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8

Minimum is the minimum amplitude of the waveform's displayed power or voltage.

The minimum level is taken directly from the histogram data. The measurement can be restricted to a measurement region. A level annotation label is placed at the minimum result. The entire screen is the interval over which the measurement is made.

This measurement may be compatible with PAM4 signals, depending on the PAM4 waveform. PAM measurement capability requires the Research and Developement or Manufacturing package license.

The measurement can be performed on any waveform that is displayed in one of a Waveform content windows.

Configurable Measurement Parameters

This measurement is not affected by setting in the Configure Base Measurements dialog.

To measure

  1. Click the toolbar's More buttons to locate the Minimum button.
  2. Click the button.
  3. If measurement regions are enabled, the Select Measurement Region, Setting dialog is displayed. Select the area over which the measurement is to be performed: a Region or the Entire Display.

SCPI Command

:MEASure:OSCilloscope:VMINimum