:TPRogram:SLINe:TEPReset
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SLINe:TEPReset "<TDECQ-EQ-preset>"
For example, "IEEE 802.3cd". Notice that the response includes double quotes.
Query Syntax
:TPRogram:SLINe:TEPReset?
Query Response
"<TDECQ-EQ-preset>"
For example, "IEEE 802.3cd". Notice that the response includes double quotes.
Description
For a Station's selected Test Program line, changes the applied TDECQ EQ Preset.
| IEEE 802.3bs |
| IEEE 802.3bs Ammended |
| IEEE 802.3cd (Covers the IEEE 802.3cu clause) |
| IEEE 802.3db/D2.0 SR (844-863 nm) |
| IEEE 802.3db/D2.0 VR (842-948 nm) |
| IEEE 802.3db/D2.0 VR (842-918 nm) |
| IEEE 802.3db/D2.0 VR (842-888 nm) |
| IEEE 802.3db/D2.0 VR (842-868 nm) |
| Fiber Channel PI - 7 Rev 0.13 |