:TPRogram:SETup:TEPReset
Flex Apps:
                                                FlexOTO
                                            FlexOTO Instance:
                                                Stations
                                            Command Syntax
:TPRogram:SETup:TEPReset "<TDECQ-EQ-preset>"
For example, "IEEE 802.3cd". Notice that the response includes double quotes.
Query Syntax
:TPRogram:SETup:TEPReset?
Query Response
"<TDECQ-EQ-preset>"
Description
When creating a Test Program for a Station, selects the  TDECQ EQ Preset to be applied to the currently selected fixtures and Lanes. To select the fixtures and lanes, use the :TPRogram:SETup:FIXTure and :TPRogram:SETup:FIXTure:LANE commands. 
| IEEE 802.3bs | 
| IEEE 802.3bs Ammended | 
| IEEE 802.3cd (Covers the IEEE 802.3cu clause) | 
| IEEE 802.3db/D2.0 SR (844-863 nm) | 
| IEEE 802.3db/D2.0 VR (842-948 nm) | 
| IEEE 802.3db/D2.0 VR (842-918 nm) | 
| IEEE 802.3db/D2.0 VR (842-888 nm) | 
| IEEE 802.3db/D2.0 VR (842-868 nm) | 
| Fiber Channel PI - 7 Rev 0.13 |