| Main Tab Commands | 
	
		| Softkey | Sub-item | SCPI | COM | 
	
		| VMC 
		 Setup... | Sweep | 
	
		| Sweep 
		 Type | 
	
		| Linear 
		 Frequency | SENSe:SWEep:TYPE | SweepType | 
	
		| CW Time | SENSe:SWEep:TYPE | SweepType | 
	
		| Segment 
		 Sweep | SENSe:SWEep:TYPE | SweepType | 
	
		| Power | SENSe:SWEep:TYPE | SweepType | 
	
		| X-Axis Point Spacing | SENSe:SEGMent:X:SPACing | XAxisPointSpacing | 
	
		| Number of Points | SENSe:SWEep:POINts | NumberOfPoints | 
	
		| IF Bandwidth | SENSe:BWIDth[:RESolution] | IFBandwidth | 
	
		| Power | 
	
		| Power On (All Channels) | OUTPut[:STATe] | SourcePowerState | 
	
		| Port Powers Coupled | SOURce:POWer:COUPle | CouplePorts | 
	
		| DUT Input Port | 
	
		| Input 
		 Port | SENSe:MIXer:PMAP | SetDutPorts | 
	
		| Power 
		 Level | SOURce:POWer[:LEVel][:IMMediate][:AMPLitude] | InputLinearPowerLevel | 
	
		| Source 
		 Leveling Mode | SOURce:POWer:ALC[:MODE] | ALCLevelingMode | 
	
		| DUT Output Port | 
	
		| Output 
		 Port | SENSe:MIXer:PMAP | SetDutPorts | 
	
		| Power 
		 Level | SOURce:POWer[:LEVel][:IMMediate][:AMPLitude] | InputLinearPowerLevel | 
	
		| Source 
		 Leveling Mode | SOURce:POWer:ALC[:MODE] | ALCLevelingMode | 
	
		| DUT Input Port Power Sweep | 
	
		| Start 
		 Power | SOURce:POWer:PORT:STARt | StartPowerEx | 
	
		| Stop Power | SOURce:POWer:PORT:STOP | StopPowerEx | 
	
		| Points | None | None | 
	
		| Power 
		 Step | None | None | 
	
		| DUT 
		 Output Port Power Sweep | 
	
		| Start 
		 Power | SOURce:POWer:PORT:STARt | StartPowerEx | 
	
		| Stop Power | SOURce:POWer:PORT:STOP | StopPowerEx | 
	
		| Path 
		 Configuration... | SENSe:PATH:CONFig:ELEMent[:STATe] | Element | 
	
		| Mixer Frequency | 
	
		| Input | SENSe:MIXer:CALCulate | Calculate | 
	
		| LO1 | SENSe:MIXer:LO:FREQuency:FIXed | LOFixedFrequency | 
	
		| Input > LO | SENSe:MIXer:LO:FREQuency:ILTI | IsInputGreaterThanLO | 
	
		| Output | SENSe:MIXer:CALCulate | Calculate | 
	
		| Mixer 
		 Power | 
	
		| Power On (All Channels) | OUTPut[:STATe] | SourcePowerState | 
	
		| LO1 Power | SENSe:MIXer:LO:POWer | LOPower | 
	
		| LO2 Power | SENSe:MIXer:LO:POWer | LOPower | 
	
		| LO1 Swept Power | 
	
		| Start | SENSe:MIXer:LO:FREQuency:STARt | LOStartFrequency | 
	
		| Stop | SENSe:MIXer:LO:FREQuency:STOP | LOStopFrequency | 
	
		| Step | None | None | 
	
		| LO2 Swept Power | 
	
		| Start | SENSe:MIXer:LO:FREQuency:STARt | LOStartFrequency | 
	
		| Stop | SENSe:MIXer:LO:FREQuency:STOP | LOStopFrequency | 
	
		| Step | None | None | 
	
		| Path 
		 Configuration... | SENSe:PATH:CONFig:ELEMent[:STATe] | Element | 
	
		| Mixer Setup | 
	
		| Converter Stages | SENSe:MIXer:STAGe | LOStage | 
	
		| Add Source... | SENSe:ROLE:DEVice | AssignSourceToRole | 
	
		| Path Configuration... | SENSe:PATH:CONFig:ELEMent[:STATe] | Element | 
	
		| Save... | SENSe:MIXer:SAVE | SaveFile | 
	
		| Load... | SENSe:MIXer:LOAD | LoadFile | 
	
		| Meas Class... |  | CALCulate:MEASure:DEFine | CreateCustomMeasurementEx | 
	
		| Quick 
		 Start... | S-Param | CALCulate:MEASure:PARameter | CreateSParameterEx | 
	
		| Balanced | CALCulate:MEASure:PARameter | BalSMeasurement BBalMeasurement SBalMeasurement SSBMeasurement | 
	
		| Other | CALCulate:MEASure:PARameter | CreateSParameterEx | 
	
		| Layout 
		 Tab Commands | 
	
		| Softkey | Sub-item | SCPI | COM | 
	
		| New Trace |  | DISPlay:WINDow:TRACe[:STATe] | View | 
	
		| New Channel |  | None | chans.Add | 
	
		| New Window |  | DISPlay:WINDow[:STATe] | Add | 
	
		| New Sheet |  | DISPlay:SHEet:STATe | None | 
	
		| Delete | TrN | DISPlay:WINDow:TRACe:DELete | None | 
	
		| ChN | SYSTem:CHANnels:DELete | RemoveChannelNumber | 
	
		| WinN | DISPlay:WINDow[:STATe] | Add | 
	
		| Select | TrN | DISPlay:WINDow:TRACe:SELect | None | 
	
		| ChN | None | None | 
	
		| WinN | DISPlay:WINDow:TRACe:SELect | None | 
	
		| Measure... |  | CALCulate:MEASure:PARameter | CreateSParameterEx | 
	
		| Meas Class... |  | CALCulate:MEASure:DEFine | CreateCustomMeasurementEx |