:MEASure:JITTer:BSCale

Command Syntax

:MEASure:JITTerN:BSCale {QSCale | BSCale}

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

Query Syntax

:MEASure:JITTerN:BSCale?

Description

Lets you display the jitter Bathtub graphs using either the Q-scale or the BER scale. The Q-scale represents a Gaussian distribution as a straight line and makes it easier to see how Gaussian the distribution is.