:MEASure:JITTer:JITTer:EOPening:PROBability
Command Syntax
:MEASure:JITTerN:JITTer:EOPening:PROBability <probability_value>
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
<probability_value> is a double.
Query Syntax
:MEASure:JITTerN:JITTer:EOPening:PROBability?
Description
When using using a probability when calculating the total jitter (TJ) and Eye Width (see :MEASure:JITTer:JITTer:EOPening), this command lets you enter the measurement probability value.