:MEASure:JITTer:JITTer:RJCValue
Command Syntax
:MEASure:JITTerN:JITTer:RJCValue <compensation_RJ_value>
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
<compensation_RJ_value> is a double.
Query Syntax
:MEASure:JITTerN:JITTer:RJCValue?
Description
When using custom RJ compensation (see :MEASure:JITTer:JITTer:RJComp), this command lets you specify the appropriate custom RJ value.