:MEASure:JITTer:JITTer:RJSTabilize

Command Syntax

:MEASure:JITTerN:JITTer:RJSTabilize {ON | OFF | 1 | 0}

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

Query Syntax

:MEASure:JITTerN:JITTer:RJSTabilize?

Query Response

{1 | 0}

Description

Enables or disables RJ stabilization, which locks (stabilizes) the value of the measured RJ that is used in jitter measurements.

Use RJ stabilization to prevent any uncorrelated non-Gaussian, non-periodic jitter from falsely contributing to any measured RJ value. One use of RJ stabilization is to prevent cross talk, from an adjacent channel, appearing as jitter.

When stabilization is on, the measurement pane shows an asterisk is shown next to the RJ (rms) measurement results warning you that the measurement result has been modified. Above the table the annotation "*RJ Fixed at:" lists the entered value.

Use the :MEASure:JITTer:JITTer:RJSValue command to specify the appropriate RJ value.