:MEASure:JITTer:JITTer:RJCResult?

Query Syntax

:MEASure:JITTerN:JITTer:RJCResult?

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

Query Response

<RJ_compensation_result> is a double value.

Description

This query returns the RJ compensation result.

When using custom RJ compensation (see :MEASure:JITTer:JITTer:RJComp), this query returns the custom RJ compensation value and is equivalent to the :MEASure:JITTer:JITTer:RJCValue query.

When using automatic RJ compensation values derived from the RN compensation (see :MEASure:JITTer:JITTer:RJComp), this query returns a value that is calculated from slew rate and noise. (RN compensation is specified by the :MEASure:JITTer:NOISe:RNComp command.)

When RJ compensation is off (see :MEASure:JITTer:JITTer:RJComp), this query returns zero.