:MEASure:JITTer:JITTer:FLAG
Command Syntax
:MEASure:JITTerN:JITTer:FLAG <ISI_filter_lag>
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
<ISI_filter_lag> is an integer.
Query Syntax
:MEASure:JITTerN:JITTer:FLAG?
Description
When an arbitrary pattern sequence is specified (see :MEASure:JITTer:JITTer:PTYPe), this command lets you specify how many lagging coefficients are contained in the ISI filter.