:MEASure:JITTer:JITTer:EDGE

Command Syntax

:MEASure:JITTerN:JITTer:EDGE {RISing | FALLing | BOTH}

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

Query Syntax

:MEASure:JITTerN:JITTer:EDGE?

Description

This command selects whether jitter measurements are made on the RISing edge, the FALLing edge, or BOTH edges (rising and falling).

Jitter measurements performed on clock-type signals typically use a single edge setting, unless both edges of the clock are used to latch data.

In double data rate applications, this control should be set to BOTH edges.