:MEASure:JITTer:JITTer:TJBer

Command Syntax

:MEASure:JITTerN:JITTer:TJBer <SER_value>

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

<SER_value> is a double.

Query Syntax

:MEASure:JITTerN:JITTer:TJBer?

Description

When using using a symbol error rate (SER) in conjunction with the Jitter Bathtub curve when calculating the total jitter (TJ) and Eye Width (see :MEASure:JITTer:JITTer:EOPening), this command lets you enter the measurement SER value.