Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:MEASure:JITTer:JITTer:NUINtervals

Jitter Setup Commands
  • :MEASure:JITTer:BSCale
  • :MEASure:JITTer:GSCale
  • :MEASure:JITTer:JITTer:ANALysis
  • :MEASure:JITTer:JITTer:DIMensions
  • :MEASure:JITTer:JITTer:DMAXimized
  • :MEASure:JITTer:JITTer:EDGE
  • :MEASure:JITTer:JITTer:EOPening
  • :MEASure:JITTer:JITTer:EOPening:PROBability
  • :MEASure:JITTer:JITTer:FLAG
  • :MEASure:JITTer:JITTer:FLEad
  • :MEASure:JITTer:JITTer:MODE
  • :MEASure:JITTer:JITTer:NUINtervals
  • :MEASure:JITTer:JITTer:PTYPe
  • :MEASure:JITTer:JITTer:RJBandwidth
  • :MEASure:JITTer:JITTer:RJComp
  • :MEASure:JITTer:JITTer:RJCResult?
  • :MEASure:JITTer:JITTer:RJCValue
  • :MEASure:JITTer:JITTer:RJSTabilize
  • :MEASure:JITTer:JITTer:RJSValue
  • :MEASure:JITTer:JITTer:SMEThod
  • :MEASure:JITTer:JITTer:TJBer
  • :MEASure:JITTer:JITTer:UNITs
  • :MEASure:JITTer:SOURce

Command Syntax

:MEASure:JITTerN:JITTer:NUINtervals <N_unit_intervals>

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

<N_unit_intervals> is an integer.

Query Syntax

:MEASure:JITTerN:JITTer:NUINtervals?

Description

When the N-Unit Interval method of extrapolating TJ from TIE measurements is selected (see :MEASure:JITTer:JITTer:MODE), this command lets you enter the value of N.