:MEASure:JITTer:JITTer:RJComp
Command Syntax
:MEASure:JITTerN:JITTer:RJComp {OFF | CUSTom | AUTomatic}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:JITTer:RJComp?
Description
This command selects the RJ compensation option:
- OFF
- Disables RJ compensation.
- CUSTom
- Enables a user-defined value for RJ compensation.
- If there are known contributors to random jitter, you can use RJ Compensation to compensate or remove jitter from the measurement results.
- Use the
:MEASure:JITTer:JITTer:RJCValuecommand to specify the appropriate RJ compensation value. - AUTomatic
- Uses the RN compensation values specified by the
:MEASure:JITTer:NOISe:RNCompcommand.