:MEASure:JITTer:JITTer:DIMensions
Command Syntax
:MEASure:JITTerN:JITTer:DIMensions <left_col>,<right_col>
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
<left_col> and <right_col> are whole or decimal numbers.
Query Syntax
:MEASure:JITTerN:JITTer:DIMensions?
Description
Specifies the proportions of the left-column statistics table and the right-column jitter graphs within the Jitter results window.
The width of a column is the number specified, divided by the sum of all the numbers specified, times the total display width. For example, to specify left and right column widths of 60% and 40%, respectively, you can use the dimensions of "0.6,0.4", "6,4", "60,40", etc.