:CALibrate:OPTical:USER:CHANnel:MPOWer
Flex Apps:
FlexDCA
FlexRT
Instruments:
N1093A/B
Command Syntax
:CALibrate:OPTical:USER:CHANnelN:MPOWer <power>
<power> is a double.
Where N identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, CHANnel3C.
Description
For devices that require a modulated optical signal as part of the calibration, this command specifies the modulated power (RMS) of the optical signal used during an N1093A/B DCA-M user optical calibration .
Requires FlexDCA revision A.07.90 and above.