:CALibrate:OPTical:USER:CHANnel:STATus:DETails?
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:OPTical:USER:CHANnel{1:8}{A|B|C|D}:STATus:DETails?
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
On DCA-M and N1000A plug-in optical modules, queries a string of status details. If a user calibration has never been performed, the following string is returned:
"This calibration has never been performed on this instrument."
Requires FlexDCA revision A.02.00 and above.
Example Returned Status String
"Time of last Calibration: 10/23/2012 11:52:00,Elapsed Calibration Time: 3 hours 2 minutes,Temperature Change: 1.24 C"
Example Command
:CALibrate:OPTical:USER:CHANnel2A:STATus:DETails?