:CMODe:CWINdow
Command Syntax
:CMODe{1:8}{A|C}:CWINdow TIMe{1}
Where the required specifier {1:8}{A|C} identifies the common-mode channel by its module slot and channel letter. For example, the common-mode waveform of channels 1A and 1B would be identified as 1A.
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CMODe{1:8}{A|C}:CWINdow?
Description
The :CMODe:CWINdow command allows you to assign a common-mode waveform to a Waveform content window.
Currently, there is only one Waveform content window, so you will not need to use this command.
In future revisions, the :CMODe:CWINdow command will select a Waveform content window in which to display a common-mode channel waveform. In FlexDCA, several different types of content windows exist. Common-mode channel waveforms can only be displayed in a Waveform (TIMe1) content window of which there is currently only one available. This command is provided for future use when more than one Waveform content window is available for use.
| Argument | Displayed Waveform Content Window |
Number of Available Windows |
Scale Units | |
|---|---|---|---|---|
| Programmatically | Via Front Panel |
|||
| TIMe1 | Waveform | 1 | 1 | Y-Axis: Volts or Watts (linear scale) X-Axis: seconds |
Requires TDR/TDT mode. Requires FlexDCA revision A.04.00 and above.
Example Command
:CMODe2A:CWINdow TIMe1