:CMODe:UDEFined:TOP
Command Syntax
:CMODe{1:8}{A|C}:UDEFined:TOP <amplitude>
<amplitude> is a double.
Where the required specifier {1:8}{A|C} identifies the common-mode channel by its module slot and channel letter. For example, the common-mode waveform of channels 1A and 1B would be identified as 1A.
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CMODe{1:8}{A|C}:UDEFined:TOP?
Description
For the indicated channel, sets or queries the custom top-level setting. The top and base levels are used to locate a waveform's lower, middle, and upper threshold levels during measurements. Specify the level in volts or Watts depending on the waveform type. Use :CMODe{1:4}:UDEFined:BASe to set or query a custom base level.
Before this custom top level can be applied to measurements, use the :MEASure:TBASe:METHod command to select custom top-base definitions.
Requires TDR/TDT mode. Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:MEASure:TBASe:METHod UDEFined :CMODe1A:UDEFined:BASe -125E-3 :CMODe1A:UDEFined:TOP 125E-3