:CMODe:YOFFset
Command Syntax
:CMODe{1:8}{A|C}:YOFFset <offset>
<offset> is a double.
Where the required specifier {1:8}{A|C} identifies the common-mode channel by its module slot and channel letter. For example, the common-mode waveform of channels 1A and 1B would be identified as 1A.
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CMODe{1:8}{A|C}:YOFFset?
Description
Sets the voltage that is represented at the center of the display for the selected common-mode waveform.Offset parameters are vertical scale dependent. Currently, the offset can be expressed in volts only using the :CMODe:UNITs command. Use the :CMODe:YSCale command to change a channel's vertical scale.
Requires TDR/TDT mode. Requires FlexDCA revision A.04.00 and above.
Example Command
:CMODe3C:YOFFset?