:CMODe:COLor

Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter

Command Syntax

:CMODe{1:8}{A|C}:COLor  {TCOLor1 | TCOLor2 | … | TCOLor16}

Where the required specifier {1:8}{A|C} identifies the common-mode channel by its module slot and channel letter. For example, the common-mode waveform of channels 1A and 1B would be identified as 1A.

The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.

Query Syntax

:CMODe{1:8}{A|C}:COLor?

Description

Selects the color used to identify a common mode waveform on the screen. Waveform color assignments are saved as part of an instrument Setup file (:DISK:SETup:SAVe). Waveform colors are reset to their default values by a default setup (:SYSTem:DEFault) or factory preset (:SYSTem:FACTory).

Channel Colors Versus Command Arguments
Color Argument Color Argument Color Argument Color Argument
TCOLor1 TCOLor2 TCOLor3 TCOLor4
TCOLor5 TCOLor6 TCOLor7 TCOLor8
TCOLor9 TCOLor10 TCOLor11 TCOLor12
TCOLor13 TCOLor14 TCOLor15 TCOLor16

To change the color of any waveform, use the following additional subsystem :COLor commands:

All :COLor Commands
Command Description
:CHANnel:COLor Sets color of channel waveforms.
:CMODe:COLor Sets color of common-mode waveforms.
:DIFF:COLor Sets color of differential waveforms.
:EMEMory:COLor Sets color of eye memory waveforms
:FUNCtion:COLor Sets color of math function output waveforms.
:TRACe:COLor Sets color of T-domain parameter or S-parameter waveforms in TDR/TDT mode.
:WMEMory:COLor Sets color of waveform memories.

Requires FlexDCA revision A.04.50 for colors 13 through 16.

Requires FlexDCA revision A.04.00 and above for colors 1 through 12.

Requires TDR/TDT mode.

Example Command

:CMODe6C TCOLor4