:CMODe:SIGNal:TYPE:AUTO
Command Syntax
:CMODe{1:8}{A|C}:SIGNal:TYPE:AUTO {ON | OFF}
Where the required specifier {1:8}{A|C}
identifies the common-mode channel by its module slot and channel letter. For example, the common-mode waveform of channels 1A and 1B would be identified as 1A
.
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A
. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CMODe{1:8}{A|C}:SIGNal:TYPE:AUTO?
Description
Turns on and off automatic detection of the signal type that is input to the specified channel. By default, automatic detection is on. When automatic detection is turned off, specify the type of signal with the :SIGNal:TYPE
parent command.
Requires TDR/TDT mode. Requires FlexDCA revision A.04.50 and above.
Example Command
:CMODe2C:SIGNal:TYPE:AUTO ON