:CMODe:SIGNal:TYPE

Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter

Command Syntax

:CMODe{1:8}{A|C}:SIGNal:TYPE {UNSPecified | NRZ | PAM4 | PAM6 | PAM8}

Where the required specifier {1:8}{A|C} identifies the common-mode channel by its module slot and channel letter. For example, the common-mode waveform of channels 1A and 1B would be identified as 1A.

The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.

Query Syntax

:CMODe{1:8}{A|C}:SIGNal:TYPE?

Query Response

{UNSP | PAM4 | PAM6 | PAM8}

Description

By default, automatic detection is turned on and is performed as part of an autoscale (:SYSTem:AUToscale). The detected format is always Unspecified.

Example Command Sequence

:CMODe2A:SIGNal:TYPE:AUTO OFF 
:CMODe2A:SIGNal:TYPE PAM4

Requires TDR/TDT mode. Requires FlexDCA revision A.04.50 and above.

Example Command

:CMODe2C:SIGNal:TYPE UNSP