:CMODe:YUNits
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
Command Syntax
:CMODe{1:8}{A|C}:YUNits {VOLT}
Where the required specifier {1:8}{A|C} identifies the common-mode channel by its module slot and channel letter. For example, the common-mode waveform of channels 1A and 1B would be identified as 1A.
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CMODe{1:8}{A|C}:YUNits?
Description
Sets or queries the common-mode waveform's vertical units.
Requires TDR/TDT mode. Requires FlexDCA revision A.04.00 and above.
Example Command
:CMODe3C:YUNits VOLT