:ECONtour:BERates

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:ECONtour{1:16}:BERates <list of BER rates>

Where the required specifier {1:16} identifies a group of contour lines.

Where <list of BER rates> is a comma-separated list of rates as described below.

Query Syntax

:ECONtour{1:16}:BERates?

Description

Creates a group of contour lines in the selected group. Up to eight contour lines can be created in one of 16 groups. The command argument is a comma-separated list of BER rates with each rate defining a contour line. When this command is sent, any current contour lines for the specified contour-line group are replaced with the BER rates listed in the argument. For example, the following command argument would result in selecting two standard and creating two custom contour lines in the Eye Contour Group Setup dialog:

:ECONtour{1:16}:BERates 1E-6,1E-12,2.4E-4,1.5E-15

The query form of the command returns the contour lines defined for the specified contour-line group.

Requires FlexDCA revision A.05.30 and above.

Example Command

:ECONtour2:BERates 1E-6,1E-12,2.4E-4,1.5E-15