:ECONtour:RJSTabilize
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:ECONtour{1:16}:RJSTabilize {ON | OFF}
Where the required specifier {1:16} identifies a group of contour lines.
Query Syntax
:ECONtour{1:16}:RJSTabilize?
Description
Turns on or off Random Jitter (RJ) stabilization for a group of eye-contour lines. When RJ stabilization is on, use the :ECONtour:RJSValue:EYE command to enter a separate value of RJ for each eye. To measure the RJ, switch the N1000A to Jitter Mode and measure the RJ while using a signal that has a short pattern. Or, measure the RJ using a separate instrument. Each eye-contour line group has its own RJ stabilization values.
Requires FlexDCA revision A.05.30 and above.
Example Command
:ECONtour2:RJSTabilize ON