:ECONtour:PSPec
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
Licensed Feature:
F-AEYE
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:ECONtour{1:16}:PSPec {BER | PROBability}
Where the required specifier {1:16} identifies a group of contour lines.
Query Syntax
:ECONtour{1:16}:PSPec?
Description
Selects eye contour lines based on BER or probablility. To enter the values for each line, use the :ECONtour:BERates command. Selecting BER indicates Bit Error Rate for NRZ signals and Symbol Error Rate (SER) for PAM4 signals.
Requires FlexDCA revision A.05.30 and above.
Example Command
:ECONtour2:PSPec BER