:ECONtour:RJSValue:EYE
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
Licensed Feature:
F-AEYE
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:ECONtour{1:16}:RJSValue:EYE{0:7} <random_jitter>
Where the required specifier {1:16} identifies a group of contour lines.
Where <random_jitter> is a double.
Query Syntax
:ECONtour{1:16}:RJSValue:EYE{0|1|2}?
Description
For Random Jitter (RJ) stabilization, sets the value of RJ for the selected eye of an eye-contour group. To measure the RJ, switch to Jitter Mode and measure the RJ while using a signal that has a short pattern. Or, measure the RJ using a separate instrument, such as a spectrum analyzer. Use the :ECONtour:RJSTabilize command to turn on or off the use of RJ stabilization.
| Command | Description | |
|---|---|---|
| :EYEl2 | Applies to eye 2/3. |
|
| :EYE1 (or :EYE) |
Applies to eye 1/2. | |
| :EYE0 | Applies to eye 0/1. | |
Requires FlexDCA revision A.05.30 and above.
Example Command
:ECONtour2:RJSValue:EYE2 1.5E-9