:ECONtour:RNSTabilize
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
Licensed Feature:
F-AEYE
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:ECONtour{1:16}:RNSTabilize {ON | OFF}
Where the required specifier {1:16} identifies a group of contour lines.
Query Syntax
:ECONtour{1:16}:RNSTabilize?
Description
Turns on or off Random Noise (RN) stabilization for a group of eye-contour lines. When RN stabilization is on, use the :ECONtour:RNSValue:LEVel command to enter a separate value of RN for each eye level. To measure the RN, switch the N1000A to Jitter Mode and measure the RN while using a signal that has a short pattern. Or, measure the RN using a separate instrument. Each eye-contour line group has its own RN stabilization values.
Requires FlexDCA revision A.05.30 and above.
Example Command
:ECONtour2:RNSTabilize ON