:ECONtour:SOURce

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:ECONtour{1:16}:SOURce  <source_waveform>

Where the required specifier {1:16} identifies a group of contour lines.

Where <source_waveform> can be one of the following:

  • CHANnel{1:8}{A|B|C|D}
  • DIFF{1:4}
  • CGMemory{1:8}
  • FUNCtion{1:16}

Query Syntax

:ECONtour{1:16}:SOURce?

Description

Selects the source waveform for the selected group of Eye Contour lines. If the source is not a valid waveform type (not an eye diagram) or the waveform is not displayed, the currently defined source for the eye-contour group will not be changed. To define the group's lines, use the :ECONtour:BERates command. To display the group's lines, use the :ECONtour:DISPlay command.

The query form of the command returns

Requires FlexDCA revision A.05.30 and above.

Example Command

:ECONtour2:SOURce CHAN3A