:ECONtour:DISPlay
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:ECONtour{1:16}:DISPlay {ON | OFF}
Where the required specifier {1:16} identifies a group of contour lines.
Query Syntax
:ECONtour{1:16}:DISPlay?
Description
Displays (ON) or hides (OFF) the selected group of eye contour lines. Hiding an eye contour group does not delete the group. You can redisplay the group and even move it to another waveform. To move the group of eye contour lines, use the :ECONtour:SOURce command. To define the group's lines, use the :ECONtour:BERates command.
Requires FlexDCA revision A.05.30 and above.
Example Command
:ECONtour2:DISPlay ON