:FUNCtion:CONStant
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:FUNCtion{1:64}:CONStant <value>
<value> is an double.
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtion{1:64}:CONStant?
Description
Sets the value of a constant that can be used as an operand for the add, subtract, multiply, and versus math operators. The constant has the same vertical scale as the associated waveform source. The default constant value is 1.
Example Command
:FUNCtion2:CONStant 1.5