:FUNCtion:COLor

Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:FUNCtion{1:64}:COLor  {TCOLor1 | TCOLor2 | … | TCOLor16}

Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtion{1:64}:COLor?

Description

Selects the color used to identify an operator's output waveform on the screen. Color assignments are saved as part of an instrument Setup file (:DISK:SETup:SAVe). Waveform colors are reset to their default values by a default setup (:SYSTem:DEFault) or factory preset (:SYSTem:FACTory).

Color Arguments

Channel Colors Versus Command Arguments
Color Argument Color Argument Color Argument Color Argument
TCOLor1 TCOLor2 TCOLor3 TCOLor4
TCOLor5 TCOLor6 TCOLor7 TCOLor8
TCOLor9 TCOLor10 TCOLor11 TCOLor12
TCOLor13 TCOLor14 TCOLor15 TCOLor16

To change the color of any waveform, use the following additional subsystem :COLor commands:

All :COLor Commands
Command Description
:CHANnel:COLor Sets color of channel waveforms.
:CMODe:COLor Sets color of common-mode waveforms.
:DIFF:COLor Sets color of differential waveforms.
:EMEMory:COLor Sets color of eye memory waveforms
:FUNCtion:COLor Sets color of math function output waveforms.
:TRACe:COLor Sets color of T-domain parameter or S-parameter waveforms in TDR/TDT mode.
:WMEMory:COLor Sets color of waveform memories.

Requires FlexDCA revision A.04.50 for colors 13 through 16.

Example Command

:FUNCtion2:COLor TCOLor1