:FUNCtion:UNAMe
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:FUNCtion{1:64}:UNAMe <string>
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtion{1:64}:UNAMe?
Description
Assigns a custom user name to a function waveform. User names are helpful because they identify what a waveform represents rather than the function name. For example, you could assign user name "Transceiver Output" to the memory 2 waveform. User names can be 25 characters or less and are displayed on the screen and on screen captures. To remove a custom user name, re-create it using an empty string.
Custom user names can by created for other waveforms using the following commands:
:CHANnel:UNAMe:CMODe:UNAMe:DIFF:UNAMe:EMEMory:UNAMe:TDR:DUT:DIFFerential:NPORt:UNAMe:TDR:DUT:DIFFerential:PPORt:UNAMe:TDR:DUT:DIFFerential:SIGNal:UNAMe:TRACe:UNAMe:WMEMory:UNAMe
Requires FlexDCA revision A.03.00 and above.
Example Command Sequence
:FUNCtion2:UNAMe "Transceiver Output"