:FUNCtion:HTRacking
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:FUNCtion{1:64}:HTRacking {AUTO | MANual}
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtion{1:64}:HTRacking?
Description
Select AUTO or MANual for horizontal offset and scaling. All math operators allow horizontal scaling.
- AUTO
- The appropriate scale and offset for the function is automatically based on the source waveform. Function scaling tracks any changes to the source scaling. Use automatic scaling mode first, then use manual scaling to make fine adjustments to the functions.
- MANual
- Turns off automatic tracking of source scaling. Use the
:FUNCtion:XPOSitionand:FUNCtion:XSCalecommands to manually set the horizontal scale and offset. FlexDCA tries to display the correct units for your function.
Example Command
:FUNCtion2:HTRacking AUTO