:FUNCtion:STATus?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Query Syntax
:FUNCtion{1:64}:STATus?
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Query Response
{AVA | UNAV}
Description
Queries the availability of a math function for use. A math function becomes available (AVA) after the function is defined using the :FUNCtion:FOPerator command. The math function does not need to be displayed to be classed as available. Available math functions are shown in the Signals Palette. A math function is unavailable (UNAV) if a function has not been created.
Use the :FUNCtion:DISPlay command query to determine if a math function output waveform is displayed.
Example Command
:FUNCtion2:STATus?